Silicon Carbide (SIC) Technology

Learn how SiC technology delivers superior control and efficiency. 

Silicon Carbide (SIC) Technology

Learn how SiC technology delivers superior control and efficiency. 

Mitsubishi Electric discovered how SiC power devices drastically improve efficiencies


Mitsubishi Electric began developing SiC technology in the 1990s, convinced of its potential to revolutionize power electronics and energy efficiency. To date, it’s the only brand of UPS that designs and manufactures its own semiconductors. Our research allowed us to know best how to control SiC-powered devices, specifically SiC UPS, for optimal reliability and efficiency. We’ve leveraged that SiC technology in our SUMMIT Series® UPS.

 

SiC Technology offers more power in a smaller footprint & greater control over the flow of electricity 


SiC is the latest in high-power semiconductor devices, disrupting the power electronics industry and creating innovative opportunities through its application in Uninterruptible Power Supply Systems. Silicon had been a preferred semiconductor material for some time now because of the greater control it provides over the electron current. The development of SiC as a Wide Bandgap material allowed semiconductors to be smaller, faster and more reliable.

 

SiC Technology creates an energy-efficient UPS across all load levels


Smaller, lighter and capable of running at higher temperatures with less power and heat loss than previous silicon-based semiconductors, SiC energy efficient UPS are just as effective at delivering the right amount of power when needed. Their design allows them to operate evenly and efficiently in high and low load situations so there’s no eco-mode (and subsequent switching) required.

 

Silicon carbide technology, coupled with three-level topology, has led to the creation of the smallest, lightest, and most efficient UPS modules in the world that deliver a better response to load transients. In true online double conversion, module efficiencies of up to 98% are achievable without the use of line-interactive technology.

Learn more about Our SiC UPS

SiC power devices are an innovative solution for a sustainable future. When applied to create an energy-efficient UPS, the dramatic reduction in power loss and significant increase in energy savings help support a low-carbon society, while delivering the same reliability and uptime as previous models. For more information on incorporating the SUMMIT Series® SiC UPS into your facility, click the button below.