Mitsubishi Electric UPS Secures Top Energy Star Ranking

Mitsubishi Electric UPS Secures Top Energy Star Ranking

About ENERGY STAR

ENERGY STAR is a government backed labeling program created by the Environmental Protection Agency in 1992 and established to identify and promote energy efficient products. 

 

It is a voluntary program and provides credible and unbiased information based on certifications by accredited independent testing organizations. Not only do ENERGY STAR-certified products reduce greenhouse gas emissions, they also save businesses significant money on energy bills.

"United States Environmental Protection Agency" plaque.
Close up of a circuit board.

Why Mitsubishi Electric?

The Mitsubishi Electric name has stood the test of time and is widely regarded as a premier brand. The power electronics market has consistently looked to Mitsubishi Electric to lead the way in advancing UPS technology and increasing efficiencies to unprecedented levels. 

Mitsubishi Electric pioneered the transformerless UPS, which led to increased efficiencies and reduced cooling requirements. Although competitors may incorporate older generation Mitsubishi Electric IGBTs in their UPS, only Mitsubishi Electric utilizes its current IGBT designs and knows best how to control these devices to squeeze out every ounce of efficiency possible.  

The Game Changer

The latest advancement introduced by Mitsubishi Electric is the use of Silicon Carbide (SiC) transistors, which achieves operational efficiencies up to 98%.

 

The use of SiC as the semiconductor material enables power switching devices to operate at much higher voltages, frequencies and temperatures than conventional semiconductor materials. All of these desirable characteristics lead to higher efficiencies.

 

Mitsubishi Electric’s SUMMIT Series® UPS is the first to incorporate SiC into its power devices and proudly sits at the top of all double conversion UPS on the ENERGY STAR website.

 

Check out this case study about UScellular deploying the high-efficiency SUMMIT Series® UPS to tremendously lower costs and secure substantial government rebates.

 

The 9900AEGIS UPS by Mitsubishi Electric is also ENERGY STAR-certified, maintaining a relatively flat efficiency curve regardless of load.

The SUMMIT Series UPS graph of efficiency.