BLOG

BLOG

Advantages of Containerized Solutions

OCTOBER 5, 2021

 

Michael Ruhe Headshot. by Michael Ruhe, Product Manager Engineered Solutions

The amount of data being transmitted and processed each year is growing with the popularity of streaming services, IoT applications, and the enterprise shift to a hybrid or cloud-based model. Over the last year and a half, the shift to a mainly remote workforce has further increased the demand placed on data centers.

 

As such, many cloud and colocation data center operators are building at a record pace and looking for every conceivable advantage that will enable deploying their resources in a quick, reliable, and cost-effective manner.

One such approach that these operators are employing is the use of modular, or pre-fab, construction and containerized power systems over the traditional stick build.

 

The space required for the future cooling and power systems needs in a traditional stick build can lead to an overall inefficient use of space and an undesirable decrease in the revenue generating white space.

 

On the other end of the spectrum, if the necessary expansion of a traditional data center outpaces the planned expansion, the data center can become undersized and cause owners to sacrifice additional potential profits.

Collage of containerized power systems on trucks and loading machines.

Modular construction and containerized designs offer many advantages that can help alleviate these concerns and should be considered when designing a new build or even upgrading an existing data center.

Blue clock icon with an arrow indicating the clock is ticking.

A modular approach provides significant benefits with regards to speed of deployment and time to market as well. The construction of the module or container occurs off site, usually at a partner integrator in parallel with the construction of the rest of facility.

 

This eliminates the risk of delays that could happen while waiting on approvals, permits, or any additional site work that could become necessary if all this construction was done in the traditional sequential manner.

Two green gears and an arrow, "reduced installation&integration time"

In addition, the time required for installation and integration will also likely be reduced.

 

Since the module or container is pre-built off site, all the testing and verification of the included systems can be performed immediately following assembly and any issues resolved more easily at the integrator’s site; i.e., the module can then arrive on site ready to be energized and quickly integrated into the data center build.

Red money bag icon with a dollar sign.

Another benefit for taking this approach can be a reduction in the upfront capital expenses associated with building the data center.

 

Standardizing on the design upfront and selecting the ideal size for your implementation means the need for overbuilding for the future growth can be eliminated on day one, reducing the stranded capacity and upfront equipment expenses. This accelerates the time to seeing positive revenue growth.

 

While there are many benefits to using the modular or containerized approach, it might not always be the best fit for a particular data center build.  For example, depending on the location of the site, increased security may be warranted and more easily achieved with a traditional facility than a container.

 

It is always best to have a discussion with your partners and vendors to evaluate the pros and cons of a modular approach on your future designs to determine the best solution for your unique application.


Stay up-to-date on industry trends & insights

Be the first notified of new blog posts

By submitting this contact form, you agree that a representative(s) of Mitsubishi Electric Power Products, Inc. (MEPPI) may contact you using the information you provided. In accordance with our Privacy Policy, we will never share or sell your personal data.

Follow us on social media

 Black and white LinkedIn icon.   Black and white Twitter icon.  Black and white YouTube icon.