The Runaway Review

Join Product Manager, JJ Hocken, as he reviews batteries and discusses the advantages and disadvantages of various chemistries impacting the UPS industry.

The Runaway Review

Join Product Manager, JJ Hocken, as he reviews batteries and discusses the advantages and disadvantages of various chemistries impacting the UPS industry.

Lithium Nickel Manganese Cobalt Oxide (NMC)

 

APRIL 17, 2023

 

Headshot of J.J. Hocken, Product Manager at Mitsbishi Electric. by J.J. Hocken, Product Manager Batteries & DC Technologies

The NMC battery, a combination of Nickel, Manganese, and Cobalt, has been a powerful and suitable lithium-ion system that can be designed for both energy and power cell applications. NMC batteries began with equal parts Nickel (33%), Cobalt (33%), and Manganese (33%)  and is known as NMC111 or NMC333. 

 

As technology and the needs in the market changed to require an increase in energy density and cobalt-reduced NMC batteries, new variants of NMC were designed. Many of the variants had increased Nickel content and decreased Cobalt and Manganese content.

 

The increase in Nickel produces energy dense batteries but can also reduce the life expectancy in some cases. The most common variants of NMC are NMC532, NMC622, and the newer NMC811.

 

Lithium hydroxide is required to make NMC811, which typically consists of 80% Nickel, 10% Manganese, and 10% Cobalt and has an increased energy density to around 200 m Ah/g.

 

Although Cobalt in the cathode of an NMC battery is used to stabilize the structure, increase battery life, and reduce cathode corrosion, an increasing number of battery manufacturers are looking to reduce the amount of Cobalt used in batteries as it can be the most problematic element due to price volatility, supply chain, and mining.

 

Cobalt is mined throughout the world; one of the largest cobalt suppliers is the Democratic Republic of Congo (DRC), followed by Russia. China leads the world in refined cobalt production at 70% of total global supply – and the material it uses comes mostly from the DRC. Cobalt mining can be very dangerous with exposure to toxic chemicals, gases, and accidents.

 

The USA has put regulations and restrictions in place to make sure certain sources of Cobalt and other minerals are not used in future supplies and designs. Estimates show that there will be a Cobalt shortage by 2028, which has been quickened by the increased use of Cobalt in electric vehicles and battery energy storage designs.

 

Lithium NMC can also be used in laptops, smartphones, and other mobile electronics. Depending on where and how the batteries are used, the NMC battery cells can be in a variety of different form types, such as cylindrical, prismatic, and pouch cells. The various cell forms and designs each have their own advantages:

 

Prismatic Cells

  • Improve space utilization and are most suitable if a flexible design is needed
  • Common in consumer electronics, energy storage systems, and electrical vehicles

Cylindrical Cells

  • Easier to manufacture and have better mechanical stability with high internal pressures
  • Tend to be more reliable in design 
  • Used in some electrical vehicles, medical instruments, laptops, e-bikes, and power tools

Pouch Cells

  • Lightweight, space efficient, and can have greater capacity
  • Can have a challenge with swelling that can be a result of gas generation during charge and discharge
  • Does have an advantage over other form factors due to its 90-95% packaging efficiency and flexible size
  • Typically requires a support enclosure or structure
  • Commonly used in vehicles, cell phones, laptops, and tablets

Advantages of the NMC battery chemistry in the UPS industry

Two green arrows moving in a circle around a lightning bolt. Increased energy/power density

 

Decreased footprint compared to Lithium Iron Phosphate (LFP) and VRLA batteries, which can reduce operation and infrastructure costs

Black outline of two sheets of paper and a feather. Lightweight, which can translate into reduced floor loading requirements

Clipart icon of a clock

Typically, a 10-year design lifespan (use case and design dependent) 

Green tag with a $ sign.

Can be cheaper in price compared to LFP and VRLA from a per UPS system standpoint

Graphic of a red thermometer.

General Operating Temperature of 25°C (77°F) +/- 5°

Red and white LiB icon with lightning bolt.

C rates fit well with UPS applications

  • Typically 0.28C to 0.55C based on design and application of the UPS (With NMC, it is preferred not to exceed 0.8C in most applications)
  • Can be charged up to 100% SOC in 30 minutes to 1 hour depending on the UPS charge output

Graphic of a green tree.

Favorable sustainability factors (GHG Emissions per average value of battery capacity)

 

Graphic of a "Test" sheet of paper and pen.

Favorable UL9540A test results for most known brands

Manageable risk of fire propagation and thermal runaway

 

Graphic of a fire extinguisher.

Typical fire suppression techniques: Excessive amounts of water, carbon dioxide, dry chemical, or foam extinguishers

 

Disadvantages of the NMC battery chemistry in the UPS industry

 

Potentially greater risk of thermal runaway if improperly used and controlled

 

Clipart icon of a clock

 

Reduced design life for batteries with higher Nickel content and reduced Cobalt content

 

Graphic of a battery next to green recycling arrows.

Overall reduced cycle life compared to LFP

 

Depending on the manufacturer, the CAPEX cost of NMC could be cheaper than LFP and many other battery chemistries. NMC does have an increased fire and thermal runaway risk, but if the NMC cells sourced are of top tier quality and are paired with a reliable and well-programed battery management system, the overall risk is minimized.

 

Lithium NMC does have a positive GHG sustainability rating. With new lithium-ion recycling methods and companies established, NMC and other lithium-ion batteries have a net substantial positive yield in recycling return.

 

New variants of NMC with reduced Cobalt chemical content in the cathode limit the dependence on Cobalt sourcing and materials. Given the nature of the NMC battery chemistry cathode design, the new Cobalt-limited NMC variants push the limits of energy-dense battery design to new heights and yields. 

 

The properties of NMC make it a solid choice for UPS applications. Many current UPS systems may cycle only three-to-five times per year depending on loads and operation within a data center.

 

NMC has increased energy density with a cycle life span that is geared towards a reduced number of cycles per year.  Typically, a NMC battery system will still have an estimated 10-year design life, which will strongly depend on the UPS use case and battery chosen.

 

NMC batteries can be a safe, reliable, and an energy-dense solution that is very well-suited for UPS applications.

Edited by Nicole Kristof, Senior Marketing Specialist


Stay up-to-date on industry trends & insights

Be the first notified of new blog posts

By submitting this contact form, you agree that a representative(s) of Mitsubishi Electric Power Products, Inc. (MEPPI) may contact you using the information you provided. In accordance with our Privacy Policy, we will never share or sell your personal data.

Follow us on social media

 Black and white LinkedIn icon.   Black and white Twitter icon.  Black and white YouTube icon.