Backup Power for Edge Data Centers

Edge data centers extend the speed and accessibility of your network - Don't let your edge data center go dark. Make sure they maintain consistent uptime with Mitsubishi Electric Uninterruptible Power Supplies.

Backup Power for Edge Data Centers

Edge data centers extend the speed and accessibility of your network - Don't let your edge data center go dark. Make sure they maintain consistent uptime with Mitsubishi Electric Uninterruptible Power Supplies.

Support your edge computing infrastructure with an uninterruptible power supply

Edge data centers are generally smaller facilities that live on the periphery of an IP network, extending the “edge” to provide computational resources to localized users.

 

They are often leveraged to deliver quicker information relays in remote locations as content doesn’t have to travel back to the hyperscale data center and back. While smaller than a traditional data center, edge centers require the same computing infrastructure - and that includes uninterruptible power supplies.

 

Give your business an edge over the competition

So, what businesses can benefit from the virtues of edge data centers?

Any business relying on near-instant data is a candidate.

 

Some of the early adopters of edge cloud computing are consumer and industrial applications, such as autonomous vehicles, artificial intelligence, gaming, and financial institutions, where a few milliseconds can make or break the profitability of a stock trade. 5G and IoT networks also benefit from the boost, especially in rural locations.

Edge cloud computing boosts the performance of your data center in rural locations.

Benefits of edge cloud computing for remote regions

Existing networks often connect to hyperscale data centers that are far removed geographically from the areas that they serve. Although very effective at number crunching, their remote locations can add precious milliseconds to transaction times and introduce undesirable latency. 

 

The switch from centralized processing to localized computing minimizes the physical gap between servers and end users and optimizes processing time. Remote locations for edge computing are typically unmanned and monitored remotely, so onsite backup power from a reliable source is even more essential to continued uptime.

 

. The switch from centralized processing to localized computing minimizes the physical gap between servers and end users and optimizes processing time.

Beyond the Buzz: The True Pulse of the Edge Data Center Market

We've been talking about the 'edge' for a few years now. But what progress has been made? Has any? Does the future of edge go beyond the buzz?

Containing the Edge

 

One approach to deploying an edge data center is through the use of containerized or pre-fab data centers, "data centers in a box," if you will.

Edge Data Centers: Why Are They Being Used?

Let's take a look as to why everyone is talking about edge data centers and why there will be a growing need in the years to come.

Edge Data Centers: Explaining the Different Types?

Typically, edge data centers are smaller data centers that live on the "edge," or periphery, of a larger network.


Edge data centers reduce permanent storage volume & conserve resources by discerning crucial data to save

The amount of data being collected is escalating exponentially, and businesses and organizations need to analyze and retain the relevant parts. Information like manufacturing metrics, environmental data, and real time retail customer store interactions are just a few examples. Transmitting all of this data to large data centers for permanent storage is not always necessary for extended record keeping.

 

Enter edge computing, capable of analyzing volumes of data and deciding how much of it needs to be stored long term, and how much can be discarded. This determination at the edge drastically reduces the essential network bandwidth and significantly releases resources at the central data center.

The importance of uninterruptible power in an edge data center infrastructure

Uptime in any data center is essential, but with more and more edge data centers leveraged for machine-to-machine (M2M) communication and IP-connected mobile devices, it could be lifesaving. Edge data centers that support M2M allow self-driving cars and other connected devices to “talk” with smart lights and other cars and get updates in real time on nearby accidents or traffic patterns.

 

If AI could impact a life, time and reliability matters exponentially more. Edge data centers support this by reducing relay time and connecting devices more quickly. Mitsubishi Electric's uninterruptible power supplies support edge computing with a clean, consistent power source that protects the uptime of the edge infrastructure against surges and outages.

Which Uninterruptible Power Supply is best for your edge data center?

With all the same operation requirements, including security, cooling, connectivity and power - but on a smaller scale - edge data centers for all types need a smaller power supply than hyperscale data centers. Operators typically need a UPS under 750kVA, with the majority of edge computing systems in the 100kVA and below range. Explore Mitsubishi Electric's Uninterruptible Power Supplies that best serve the various types of edge data centers.

 

 

On Premise Edge & Network Towers

*Mitsubishi Electric's single-phase UPS

 

On Premise Edge, Network Towers, Network Aggregation, & Network Core

 

Network Core & Regional Edge

*ENERGY STAR-rated

 

Regional Edge

*best-selling UPS in the 250.1-500 kVA range

Let's discuss

Contact us to discuss your edge power supply requirements and how Mitsubishi Electric can support your edge infrastructure.