Technologies

With its unrivaled expertise in electronics design, control, and manufacture, Mitsubishi Electric delivers the highest reliability and highest efficiency in uninterruptible power supplies.

Technologies

With its unrivaled expertise in electronics design, control, and manufacture, Mitsubishi Electric delivers the highest reliability and highest efficiency in uninterruptible power supplies.

Leadership History

Mitsubishi Electric has been at the forefront of technological advances in the design and development of uninterruptible power supplies for the past 25+ years.

 

Older UPS installations used transformer designs and Silicon-Controlled Rectifiers (SCRs) as power devices, which limited efficiencies to the 85-90% range. In the decade that followed, Mitsubishi Electric led the charge to drastically improve efficiencies with a series of revolutionary developments.

 

The introduction of Insulated Gate Bi-Polar Transistors (IGBTs) delivered higher switching rates, and, with proper control, a more refined sine wave that provided better response to load transients. Mitsubishi Electric is the only brand of UPS that designs and manufactures its own semiconductors – knowing best how to control power electronics for highest reliability and maximum efficiency.

 

The use of IGBTs inspired the concept of the 3-level topology transformerless UPS, which Mitsubishi Electric pioneered in 2008 with its 9900 series. Later, Mitsubishi Electric extended its development of SiC technologies into the MOSFET power devices used in the SUMMIT Series®, a game-changing UPS introduced in 2015. Mitsubishi Electric’s latest advancement has been the launch of the world’s first 2 megawatt capacity UPS in 2017, the 9900CX UPS and now the 9900D UPS.

 

 

Black symmetrical flock of geese flying with a red one in the front.

3 Level Topology

Three level topology provides the base building blocks to create UPS products that are capable of >97% true online double conversion efficiency.

 

First introduced to the North American UPS Market in 2008 in the 9900A series 3 phase UPS modules, Mitsubishi Electric now includes 3 level topology in all of its 480V UPS products. Mitsubishi has led the way in this technology and now has over ten years of experience in its design, construction, and operation.

3 level vs 2 level topology waveform.
Diagram showing double conversion-fully protected.

Double Conversion vs. Line Interactive

In a true online double-conversion UPS, the inverter is always on, supplying a clean, reliable power supply.

 

Double conversion UPS modules take incoming utility power, filter it, convert it to DC, and then convert it back to a perfect AC output from the inverter. This helps protect the critical load from any voltage anomalies better than line interactive UPS modules operated via a secondary, unregulated power path.

Silicon Carbide Power Electronics

Mitsubishi Electric began developing SiC technology in the 1990s, convinced of its potential to revolutionize power electronics and energy efficiency. Our research allowed us to know best how to control SiC-powered devices, specifically SiC UPS, for optimal reliability and efficiency. 

 

Silicon Carbide (SiC)-powered devices have less power loss and greater energy savings. Mitsubishi Electric now leverages the technology to achieve energy-saving results in our highly efficient, ENERGY STAR-rated UPS, the SUMMIT Series®.

3 credible quotes about emerging SiC technology.
Mitsubishi Electric 9900B UPS, open to show inside.

Virtual Neutral and the Transformerless UPS

The removal of the transformer from UPS modules is the key to achieving superior efficiencies.

 

In order to do this, key elements of UPS design must be reviewed, such as harmonic content, system fault tolerance, negative and zero sequence currents and system grounding stability.

 

Mitsubishi Electric’s Virtual Neutral provides the means to remedy all the adverse conditions that can be caused in a transformerless UPS, while providing harmonic mitigation that is unparalleled in the UPS industry.

 

This creates the perfect environment for the removal of excess transformers from the critical power path, greatly increasing overall UPS efficiency and reducing UPS footprint.

System Configurations

There are many UPS configurations available when designing a critical load application. The complexity of each design varies based upon budgets, uptime requirements, risk aversion, maintenance plans, and existing infrastructure. These designs are typically broken down into four tiers. Each tier expands on the reliability and maintainability of the previous tier.

Tier 1 chart of a single module system UPS configuration (N).

Tier I

Single Module System (SMS) operating at the needed capacity, also known as an “N” configuration.

Tier 2 chart of a multi-module system UPS configuration (N+1).

Tier II

An additional UPS is added in either an isolated redundant or a Multi-Module System (MMS) configuration, also known as “N+1” configurations.

Tier 3 chart UPS configuration (N+1).

Tier III

Distributed redundant design techniques allow for concurrent maintainability of the site. These designs allow any system to be maintained without exposing the load to unprotected power.

Tier 3 chart of "2N" or "2N+1" UPS configurations.

Tier IV

This configuration maximizes fault tolerance of the site by providing multiple UPS system power paths to the load called “2N” or “2N+1” configurations.

Each Tier has different advantages and disadvantages and choosing the right one for you can be difficult.