*Per the ENERGY STAR website when tested in VFI mode
*Per the ENERGY STAR website when tested in VFI mode
The next generation of power semiconductor is here! In the SUMMIT Series® UPS, the Si (silicon) IGBT is replaced with advanced capability SiC (Silicon Carbide) semiconductors.
The IEEE states that silicon carbide is to the 21st century what silicon was to the 20th century. Mitsubishi Electric began development of SiC semiconductors during the early 1990s and now offers this proven technology in the SUMMIT Series® UPS.
Higher efficiencies are achieved across all load levels with SiC’s lower switching losses, higher switching frequencies, and improved thermal conductivity range.
The SUMMIT Series® UPS is lithium-ion, VRLA, VLA, and Pure Lead compatible for greater flexibility.
Mitsubishi Electric delivers the highest reliability among backup power equipment suppliers. Our robust technology is designed to deliver continuous power in the most demanding environments – and it’s not just estimated. The SUMMIT Series® of uninterruptible power supplies have a sustained load carrying capacity of 99.9995% of their actual operational history.
This model features the revolutionary use of silicon carbide (SiC) semiconductors – a unique property that unleashes the power within and delivers the highest efficiencies yet (up to 98%) of any UPS on the market. This next generation technology has resulted in the creation of the smallest, lightest, and most efficient UPS modules ever developed, as demonstrated in Mitsubishi test labs and in independent test labs utilized by the ENERGY STAR program.
One of the unprecedented efficiencies of the SUMMIT Series®‘ next generation technology is reduced power loss. SiC possesses approximately 10 times the critical breakdown strength of Silicon (Si), enabling a large reduction in electrical resistance and, in turn, reduces power loss.
The SUMMIT Series® UPS creates more white space by minimizing the gray space it occupies. It can handle the same load in a significantly smaller footprint than competitive models, meaning more space can be allocated to revenue generation. The SUMMIT also has higher power density than comparable UPS, maximizing power output while minimizing gray space.
With industry-leading efficiency, the SUMMIT Series® Uninterruptible Power Supply from Mitsubishi Electric is the ideal backup power solution for colocation and large enterprise data centers across various markets.
Application | Markets |
The next generation SiC power modules featured in Mitsubishi Electric’s SUMMIT Series® UPS deliver the highest efficiencies on the market, as certified by ENERGY STAR. Deploy this cutting-edge technology and see how SUMMIT Series® could lower your data center’s total cost of ownership and PUE.
Application | Market |
Communications | Content Delivery & Media |
Ensure consist content delivery in the face of a utility power outage with the SUMMIT Series® UPS. Available in 500 and 750 kVA, this model reliably and efficiently protect your telecommunications network.
|
|
The SUMMIT Series® revolutionary use of SiC in its semiconductors unleashes the power within and delivers the highest efficiency of any true online double conversion uninterruptible power supply on the market – verified by ENERGY STAR testing.
In addition, Mitsubishi Electric’s superior expertise in optimizing power device control is proven by the flatness of this system’s efficiency curve, demonstrating high performance across all load levels.
Please note that all efficiency curves published on this site are for the respective UPS operating in true online double conversion (aka VFI).
Mitsubishi Electric offers various DC power solutions with both lithium-ion and VRLA battery cabinets, which you can learn more about below. With respect to lifespan and operation efficiency, lithium-ion batteries now outlast traditional VRLAs. They’re also getting smaller, with the BCL04-CB cabinets being the perfect size to support applications that require a small footprint. For a deeper dive into all possible solutions, review our UPS Batteries & DC Solutions.
Read the unique stories of our valued customers and discover why Mitsubishi Electric was chosen to protect their critical infrastructure.
This revolutionary system is readily equipped to maintain critical power across multiple applications. Mitsubishi Electric can customize a complete and seamless backup solution to suit your needs.
Review the various UPS peripherals including maintenance bypasses, DC energy solutions, & communication options below.
Lithium-ion
Lead Acid Battery Cabinets
Lead Acid Batteries