BLOG

Precision is Power: How Remote Sensors Deliver Smarter Cooling for High-Density Loads

FEBRUARY 19, 2026

 

Headshot of employee, Chris Soh. by Chris Soh, Product Manager IT Cooling Systems

Data centers are intricate ecosystems, and maintaining precise environmental conditions is critical to their performance. Among the biggest challenges operators face is data center thermal management.

 

The relentless thermal energy generated by racks of servers can degrade performance, shorten equipment lifespan, and cause costly interruptions – which is why modern data centers must take a targeted approach to efficient data center cooling and environmental control.

Why Environmental Control Can’t Be an Afterthought

In data center thermal management, temperature and airflow optimization are two sides of the same coin.

  • Temperature fluctuations can trigger unplanned downtime and expensive repairs
  • Pressure imbalances disrupt airflow, reduce cooling efficiency, and create hotspots that threaten uptime.

This is why cooling today is no longer about “chilling the room.” Instead, it’s about delivering precise, responsive, and efficient cooling at the rack, aisle, and zone levels.


3 Key Approaches to Precision Cooling

Modern facilities increasingly rely on three foundational approaches to data center thermal management:

  • Airflow optimization – directing air exactly where it’s needed to eliminate hotspots.
  • Precise temperature control – keeping conditions stable across racks and aisles.
  • Dynamic cooling distribution – matching cooling output to real-time, localized demand.

To promote efficient and precise data center cooling, MEWALL thermal wall systems handle temperature control via individual unit sensors and remote in-space sensors.

 

Each control option comes with trade-offs in accuracy, speed of response, energy efficiency, redundancy, and system coordination.


Which Data Center Remote Temperature Sensor Strategy Is Right for You?

Individual Unit Sensors

Each MEWALL is equipped with built-in sensors that monitor the return air temperature and the supply air temperature and then send that information to the unit’s controller.

Remote In-Space Sensors

Remote temperature sensors throughout the data hall deliver the clearest picture of true rack conditions and the most control; however, they require a more deliberate strategy to efficiently implement.

 

 

Feature Individual Unit Sensors Remote In-Space Sensors
Location of Measurement Inside each unit’s return section In front of heat sources (pods/racks)
Accuracy of Load Detection Low – limited to unit intake High – measures where heat is generated
Response to Local Load Fast but only at intake Fast – detects zone-level changes
Cooling Delivery Precision Poor – prone to mismatches Excellent – matches cooling to actual need
Redundancy Low – failure impacts operation High – majority logic mitigates drift
System Coordination None – units act in isolation Zone-level optimization
Energy Efficiency Low – risk of inefficiency High – minimizes waste
Thermal Uniformity Poor – uneven temperatures likely High – consistent across zones

 


Customizing Control with Remote In-Space Sensors

Deploying remote in-space sensors unlocks advanced control modes. But they aren’t one-size-fits-all—the right choice depends on workload density, application mix, and operational goals. Here’s how the main strategies (Averaging, Max/Min, and Zonal Control) stack up:

 

Averaging Control (Whole Group) Max/Min Control (Whole Group) Zonal Control
How it works Multiple sensors across the cold aisle are averaged by the controller The system adjusts airflow/cooling based on the hottest (and sometimes coldest) sensor reading White space is divided into zones (aisles, rows, or rack clusters), each with its own sensors and thermal wall controls
Advantages Simple, stable, energy-efficient in uniform environments
  • Prevents hot spots
  • Helps keep IT equipment within the recommended ASHRAE TC 9.9 thermal guidance
  • Highly efficient
  • Avoids overcooling entire rooms for one problem aisle
  • Adapts to modular and mixed environments
Limitations Can mask hotspots; less effective for high-density AI/ML clusters

Energy-inefficient if only a few racks run hot; can cause control “hunting.”

  • Control “hunting” means the system keeps overreacting to the hottest or coldest sensor at any given moment. For example, if one rack briefly spikes in temperature, the system ramps up cooling for the entire group. Once that rack cools down, it cuts back — only to ramp up again when another sensor shows a spike. This constant up-and-down adjustment wastes energy, creates instability, and can lead to uneven conditions across the room.

More complex to design/commission; requires advanced control logic

Best Fit Enterprise or smaller colocation facilities with even load distribution Colocation data centers or mixed-density spaces where SLA compliance requires no rack to exceed thresholds Hyperscale, high-density colocation, or AI-driven data centers with diverse workloads

 

Zonal Control

Why Pressure Control Still Matters

Temperature often gets the spotlight in cooling discussions, but airflow pressure control is just as critical. Without it, facilities risk recirculation or bypass air, which wastes energy and creates unstable conditions.

 

MEWALL offers two pressure control strategies that can be deployed depending on site needs: Constant Airflow Rate (Constant CFM) and Constant Differential Pressure Control. Both safeguard airflow integrity, reduce energy consumption, and help maintain stable operating conditions.

 

  Constant Airflow Rate (Constant CFM) Constant Differential Pressure Control
How it works

Pressure transducers are installed before and after the fan to measure static pressure.

 

This pressure reading serves as a proxy for airflow, and the system adjusts fan speed (faster or slower) to maintain a consistent CFM.

The system measures static pressure between high-pressure zones (e.g., cold aisle/front of servers) and low-pressure zones (e.g., hot aisle/rear of servers).

 

  • If the differential drops below the target, fans speed up to boost airflow.
  • If it rises above the target, fans slow down to restore balance.
Benefit Provides stable airflow delivery even as filters load or system resistance changes, ensuring predictable cooling performance Maintains proper separation between hot and cold aisles, minimizing recirculation and hot spots
Best Fit Data halls with steady, predictable airflow requirements High-density or variable-load environments where airflow demand shifts frequently

Summary

As data centers densify—driven by AI/ML, cloud, and high-performance computing—the margin for error in cooling is shrinking. Simply supplying cold air is no longer enough. Operators now need:

  • Smarter sensing
  • Granular controls
  • Purpose-built strategies that match their workloads
  • System resilience (robust designs, redundancy, and reliability)

Precision cooling isn’t optional. It’s the foundation of competitive advantage.

With its flexible sensing options and advanced thermal wall architecture, MEWALL gives operators the tools to stay ahead of thermal risks while reducing energy waste.

 


 

  Edited by Matt Slippy, Marketing Specialist & Nicole Wenger, Senior Marketing Specialist


Stay up-to-date on industry trends & insights

Get the critical power insights you need to keep your business from going dark.

By submitting this contact form, you agree that a representative(s) of Mitsubishi Electric Power Products, Inc. (MEPPI) may contact you using the information you provided. In accordance with our Privacy Policy, we will never share or sell your personal data.

Follow us on social media

 Black and white LinkedIn icon.   Black and white YouTube icon.