BLOG

Understanding Data Center Cooling Technology: From Legacy Systems to High-Density Solutions

JULY 16, 2025

 

Headshot of employee, Chris Soh. by Chris Soh, Product Manager IT Cooling Systems

In today’s data center operations, cooling is far more than just a technical consideration—it plays a vital role in ensuring performance, uptime, and energy efficiency.

 

With increasing rack densities and evolving IT demands, choosing the right data center cooling solution has become more important than ever. Poor cooling decisions can lead to costly downtime, inefficient energy use, and limit your data center’s ability to scale for future growth.

 

In this post, we’ll take a closer look at four of the most common data center cooling technologies: CRAC, CRAH, thermal wall, and RDHx.

 

Data Center Cooling Methods Overview

  • CRAC units use a refrigerant-based direct expansion (DX) system with indoor evaporator coils and outdoor condensers to remove heat.
  • CRAH and Thermal Wall units rely on chilled water systems, supplied by central chillers, circulating cold water through coils to cool air before it’s delivered to the IT equipment.
  • RDHx is a rack-level cooling solution that replaces rack doors with water-cooled heat exchangers, directly removing heat at the source.

 


CRAC (Computer Room Air Conditioners) Units

CRAC units are commonly found in small to medium-sized or legacy data centers where simplicity and self-contained cooling are preferred.

 

They are ideal where infrastructure investment needs to be minimal or where chilled water systems are not yet in place.

 

Rendering of server rooms with arrows showing airflow between servers and CRAC units.

 

Advantages of CRAC

  • Simple installation and operation as a self-contained unit.
  • No need for extensive chilled water piping or central plant infrastructure.
  • Easier to deploy incrementally in existing facilities.

 

Limitations of CRAC

  • Lower cooling capacity (up to ~100 kW per unit), making them less suited for large or high-density data centers.
  • Typically less energy efficient compared to chilled water systems.
  • Maintenance includes refrigerant handling and condenser upkeep

CRAH (Computer Room Air Handler) Units

CRAH units are preferred in larger data centers with existing chilled water infrastructure.

 

They are suitable when scalable data center cooling and operational efficiency are priorities, especially in facilities that can support central chiller plants and extensive water distribution systems.

 

Rendering of data center showing airflow from servers to CRAH units.

 

Advantages of CRAH

  • More energy-efficient than CRAC units due to the use of chilled water.
  • Larger capacity units (up to ~250kW per unit) suitable for moderate to large data halls.
  • Fewer moving parts compared to refrigerant-based systems, potentially reducing maintenance.

 

Limitations of CRAH

  • Requires robust chilled water piping, pumps, and central plant infrastructure, meaning a higher Capex.
  • Often dependent on raised floor designs with perforated tiles for air distribution.
  • Return air is typically taken from the top of the unit, which can constrain data hall layouts.

Thermal Wall Units

Thermal wall technology is a popular choice in high-capacity, modern data centers where airflow efficiency and space optimization are top priorities.

 

Unlike traditional standalone cooling units, thermal walls are built directly into the structure—typically along one side of the data hall, such as at the end of a cold aisle—next to a dedicated equipment corridor.

These systems pull hot air from a rear return plenum or corridor and deliver cooled air uniformly across the space.

 

This integrated setup allows for more precise airflow control and helps prevent hot and cold air from mixing, which can significantly impact cooling performance.

 

With fans arranged in a stacked, modular array that forms a continuous wall, thermal wall systems offer high airflow capacity while saving valuable floor space.

 

Their design supports flexible room layouts and makes them especially well-suited for large-scale data centers where CRAH units alone may not provide sufficient cooling or energy efficiency.

 

Rendering of data hall with back of Mitsubishi Electric's themal wall cooling the racks.

 

Advantages of Thermal Walls

  • High cooling capacity (500 kW+ per unit), allowing fewer units to cover large areas.
  • Stacked, modular design supports scalable airflow and capacity adjustments.
  • Integrated wall placement frees up valuable floor space and removes the need for raised floors and perforated tiles.
  • Pulls hot return air from a dedicated mechanical corridor, improving thermal isolation and airflow efficiency.
  • Supports flexible room layouts by separating hot and cold air paths, simplifying containment and space planning

 

Limitations of Thermal Walls

  • Requires mechanical corridors or dedicated spaces for hot air return.
  • More complex installation compared to traditional CRAH units.
  • Initial infrastructure costs can be higher (usually offset by operational savings in large data halls).
Rendering of Mitsubishi Electric's MEWALL showing internals.

RDHx (Rear-Door Heat Exchanger)

RDHx have been around for a while but saw limited adoption in the past.

 

However, with the rise of ultra-high-density deployments—particularly in AI clusters, hyperscale data centers, and High-Performance Computing (HPC) environments—RDHx is gaining renewed attention as a practical and efficient solution.

 

By cooling air at the rack level, RDHx reduces or eliminates the need for traditional room-level airflow management, making it an increasingly attractive option in today’s evolving thermal landscape.

 

Image of black RDHx made by RC and Mitsubishi Electric.

 

Advantages of RDHx

  • Cools servers directly at the rack, improving heat transfer efficiency.
  • Can be added to a liquid cooling system to help cool the entire rack. While cold plates handle the chips, RDHx cools other components like power supplies and memory. This combination reduces or eliminates the need for traditional air cooling in the data center.
  • Enables higher chiller water temperatures, improving chiller efficiency and reducing energy costs.

 

Limitations of RDHx

  • Higher upfront costs due to more complex rack components and cooling plumbing.
  • Increased fan power consumption as multiple smaller fans are used instead of fewer large ones.
  • May require Coolant Distribution Units (CDUs) to regulate liquid flow and temperature, adding to system complexity.
  • Partial room cooling with RDHx requires integration with other cooling methods.


Cooling Efficiency & Airflow Containment

While system efficiency is a key consideration when evaluating data center cooling technologies—such as CRAC, CRAH, or thermal wall units—it’s important to recognize that efficiency isn’t driven by the technology alone.

 

A major source of inefficiency in data center cooling systems comes from air mixing, where hot exhaust air and cold supply air blend, reducing cooling effectiveness. 

 

Graphic of 2D birds-eye view of data hall showing air mixing due to no aisle containment.

 

To combat this, containment systems are implemented to isolate airflow paths.

 

Graphic of 2D birds-eye view of data hall showing no air mixing thanks to aisle containment.

 

There are two main types of containment:

 

Rendering of data hall showing hot aisle containment.

Hot Aisle Containment

This method encloses the hot air exhaust aisle, preventing it from mixing with cold supply air.

 

It requires a specific ceiling design and is therefore better suited for new builds rather than retrofits.

 

 

Cold Aisle Containment

This setup encloses the cold supply aisle to keep cold air focused where it’s needed. However, because the aisle is sealed, accessing equipment inside can be harder during maintenance.

 

As a result, some operators may avoid fully enclosing the aisle or leave doors open, which reduces the system’s efficiency.

 

Modern greenfield data centers benefit from efficient cooling and even temperature distribution. Advanced solutions, like Thermal Wall technology, eliminate the need for cold aisle containment. Instead, they rely solely on hot aisle containment for both efficiency and ease of operation.


Summary

  • CRAC units are best for smaller or legacy sites prioritizing simplicity.
  • CRAH units fit well in larger facilities with chilled water infrastructure aiming for efficiency.
  • Thermal Walls deliver high capacity and flexible layout options for modern, large data centers.
  • RDHx offers rack-level cooling for ultra-high-density environments, complementing primary liquid cooling systems to enhance overall efficiency and scalability in high-demand applications.

Airflow containment helps eliminate air mixing, improving cooling efficiency, which is why modern data centers include airflow containment strategies in their infrastructure to reduce long-term operating costs.

 

Today’s data centers are facing greater heat loads and energy efficiency pressures than ever before – and not all cooling methods can keep up.

 

Cooling has quickly become a strategic component of data center design. Whether you’re managing a legacy facility or building a hyperscale environment from the ground up, understanding the strengths and trade-offs of CRAC, CRAH, thermal wall, and RDHx systems is essential.

 

By aligning cooling strategies with operational goals, infrastructure capabilities, and future growth plans, operators can ensure both performance and sustainability.


Don’t Let Your Business Go Dark®

As data center cooling technology evolves, staying informed and adaptable will be key to maintaining efficient, resilient data centers.

 

Mitsubishi Electric delivers advanced, proven data center cooling solutions that help you stay ahead. Talk to our experts to customize a scalable, efficient system to best suit your needs!

 

  Edited by Matt Slippy, Marketing Specialist & Nicole Kristof, Senior Marketing Specialist


Stay up-to-date on industry trends & insights

Get the critical power insights you need to keep your business from going dark.

By submitting this contact form, you agree that a representative(s) of Mitsubishi Electric Power Products, Inc. (MEPPI) may contact you using the information you provided. In accordance with our Privacy Policy, we will never share or sell your personal data.

Follow us on social media

 Black and white LinkedIn icon.   Black and white YouTube icon.